is possible to communicate with KIT33771TPLEVB directly on SPI from micro controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

is possible to communicate with KIT33771TPLEVB directly on SPI from micro controller

1,218 次查看
sujendra_n2
Contributor I

Hello,

Please let us know whether it is possible to communicate with KIT33771TPLEVB directly on SPI from micro controller instead of TPL mode through Transceiver. We have ordered the transceiver but stock is not available it seems. So we decided to work on SPI mode till Transceiver is available.

And as all SPI pins are not populated from KIT33771TPLEVB can we directly solder a wire from 33771 chip from HW experts ? or Do you suggest any alternate method? Please reply us soon as our work is getting delayed

Thanks in advance

Thanks and Regards

N Sujendra

标签 (1)
0 项奖励
回复
1 回复

936 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Thank you for writing.

I do not know if you are still having a problem. Unfortunately, the information that you are requesting is confidential. If you want more information, you need to create a case.

On this webpage you can create a case.

NXP TechSupport Community 

Thank you for writing.

Best Regards,

Diego.

0 项奖励
回复