Thanks Tomas,
I thinking about how calculate relative acceleration with ZSTAR3 but in my opinion this is immposible. You are right Thomas.
With this sensor I have only tilt and absolute acceleration in X,Y,Z-axis.
I can only calculate relative acceleration when i let go down without rotation. Then I can choose with all date
max acceleration and min acceleration(1g) and calculate relative acceleration = max acceleration - min acceleration(1g) in Z-axis.
But when I let go down and sensor is in position X-axis 45 degrees and Z-axis 45 degrees ( photo below) I can't calculate relativ acceleration
in X or Z direction.
I measure with this construction (photo) acceleration of falling sensors and angle of sensor is in X,Z-axis 45 degrees.
Of course i want to measure relative acceleretion in X,Z-acceleration
Maybe someone have different opinion?
Best regards
Adek