Working condition with MPXV5100DP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Working condition with MPXV5100DP

1,456 Views
eldadchen
Contributor I

Hi,

we have a system that produce both pressure and vacuum.

according to the spec, this sensor can measure only pressure, and its graph starts from 0kPa (although the voltage doesn't, 0kPa=0.2V).

  • If the sensor is under vacuum state, can it harm it?
  • While putting the system under vacuum state, we got a reading from the sensor, that match the vacuum level. can we use this reading and count that other sensors will give the same reading, although the sensor graph in the spec doesn't show this side of the sensor? (we want to use the range of 0-0.2V)

Thank you,

Eldad

0 Kudos
1 Reply

1,353 Views
darioarias
NXP Employee
NXP Employee

Hi Eldad,

The MPX5100DP will not be damaged as long as the pressure in port one is greater than pressure in port two (P1>P2). Hence if you leave P1 exposed to the atmosphere, then you can go as low in P2 as 100kPa, after that, the device would be saturated and would only provide an output of ~4.7v.

Since this is a differential pressure sensor, the reading you got from the sensor will match the vacuum level so, I can confirm to you that this will work for any other MPX5100DP.

Regards,

Dario

0 Kudos