What is the proper method for retrieving samples from the CRTouch using the FIFO?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the proper method for retrieving samples from the CRTouch using the FIFO?

902 Views
wildhorsemusic
Contributor III

Hello,

After reading the CRTouch Datasheet, I am not sure how the FIFO buffer gets read using interrupts.  I understand that the FIFO watermark can trigger an interrupt to the CPU. But, once the FIFO interrupt has occurred and you send the command to read the FIFO buffer; what is the method for reading the FIFO so that the CPU doesn't run ahead of the 100Kbs rate of the CRTouch?  I would like to use an interrupt method, but it looks like I have to use a polling method, is that correct?

The docs don't give a description of reading the FIFO.  Maybe I'm missing something basic... my apologies in advance.

Duane

Labels (1)
0 Kudos
Reply
1 Reply

668 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Duane Owens,

You are correct, unfortunately it is not possible to read the FIFO buffer using Interrupt method, you would need to use a polling method to read it.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply