Hi, I have to design a device to measure the vibration on the splindle of mechanical machine. I already used the MMA8451 accelerometer to measurement of inclination; for us, could I use it also to measure the vibration? Best regards.
Hi Mauro,
The MMA8451Q might be a good choice, but we need more information such as the frequency of vibration, since vibration sensing is limited by an internal filtering in an accelerometer.
Best regards,
Tomas
The spindle can run at 30000 rpm so the frequency is 500 Hz