TPMS - FSLTMPSRCV8000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TPMS - FSLTMPSRCV8000

2,189 Views
nick_the_master
Contributor I

Hello,

I'm from the technical university Clausthal.

In the past we got some samples of the tire pressure measurement system. We got 4 sensors and one device that can be connected to the PC via USB.

Unfortunately we did not got any documentation abaout this so I have some serious trouble getting this to work.

My broblem is that i am not able to get any information about this "FSLTMPSRCV8000".

Pluged into the PC it is an unknown device VID_C1CA&PID_0005.

Can anyone tell me what device actually is and how i can use it?

Thanks

Labels (1)
0 Kudos
1 Reply

1,999 Views
david_diaz
NXP Employee
NXP Employee

Hello Nicholas,

I will be helping you at the Technical Service Request 1-4194544644.

Any update about your issue, please refer to the service mentioned.

Thank you for your interest in Freescale.

Have an excellent.

David

0 Kudos