FXAS21002C: HPF and LPF=12.5Hz

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FXAS21002C: HPF and LPF=12.5Hz

1,194 次查看
riscypayne
Contributor I

Hi Is there guideline how to choose or select HPF and LPF function for given application?

I'm using ODR = 12.5Hz and application is directional.

Would HPF reduce the drift or offset readout?

R.

标签 (1)
0 项奖励
回复
1 回复

877 次查看
anthonyduhamel
NXP Employee
NXP Employee

Hello Rlscy,

LPF cutoff frequency with an 12.5Hz ODR is fixed to 4Hz.

Ftabs.PNG

You can enable the HPF filter by setting the HPF_EN bit in the CTRL_REG0. The HPF filter should remove/attenuate the average value (offset) of the ouput signals.

Anthony

0 项奖励
回复