TEF82xx CSI2 frame

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEF82xx CSI2 frame

1,784 Views
shansshi
Contributor I

TEF82xx CSI2.pngHello:

we use the TEF82xx,It is used as FMCW RADAR transceiver.
And  we want to take the raw data to the fpga by the csi2. So we want to know the bits of the SoT、FS、EoT、PH、PF、FE、and so on.

 

Thank you.

0 Kudos
Reply
4 Replies

1,705 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

As the TEF82xx information are mostly confidential it is not the best place to communicate it via community. If you are asking for such information, it is better to submit ticket on NXP web.

Have a look at reference manual of TEF82xx

chapter 4.2.2.7 CSI2 payload packet format and chapter 4.2.1.3 LVDS data format

Best regards,

Peter

0 Kudos
Reply

1,778 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you share more info on this. Which micro you are referring to? Are you using Radar SDK?

Best regards,

Peter

0 Kudos
Reply

1,747 Views
shansshi
Contributor I

Hello,

        Can you give some infomation about our plan?

 

Thank you.

        

0 Kudos
Reply

1,770 Views
shansshi
Contributor I

Hello:

RF:TEF82xx.

FPGA:Lattice MD6000 or Xilinx XAZU5EV-1SFVC784Q, It is Connected with RF through the CSI2.

And we do not use Radar SDK.

So we want to know the frame protocol of the CSI2, for example the bits of the SoT、FS、EoT、PH、PF、FE, and so on.

0 Kudos
Reply