TEF82xx 77 GHz AUTOMOTIVE RADAR TRANSCEIVER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEF82xx 77 GHz AUTOMOTIVE RADAR TRANSCEIVER

3,161 Views
sam16
Contributor I

I had some questions about the TEF82xx 77 GHz AUTOMOTIVE RADAR TRANSCEIVER. In the fact sheet, no info about weight and range has been mentioned. Can someone help me out?

0 Kudos
Reply
1 Reply

3,142 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am a bit confused by your question as this depends on antenna design.

Radar Max Range is determined, ideally speaking, on the properties of the antenna only. A signal at a certain frequency is transmitted, reflected, then hopefully, detected. Due to the three-dimensional propagation of radar waves, frequency hold the highest weight in determining range.

The TEF82xx car RADAR transceiver is a single-chip automotive FMCW RADAR transceiver for short-range, medium-range, and long-range RADAR applications, covering the full 76 GHz to 81 GHz automotive RADAR frequency band.

petervlna_0-1637829118256.png

Best regards,

Peter

 

0 Kudos
Reply