Should I remove the gravity?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Should I remove the gravity?

1,607 次查看
zhangjive
Contributor I

Hi, 

       I want to install a accelerometer on the car's suspension, the accelerometer is used to measure the vibration result from uneven road surface. I'm afraid that the gravity will affect the accelerometer's measurements when car goes up or down a slope. So,  I have two questions:

        1. Should I remove the gravity from the accelerometer's measurements?

        2. If I have to remove the gravity, is there any method to remove that?  I only have a 3-axis accelerometer.

         Looking forward your reply.

         Thanks a lot! 

标签 (1)
0 项奖励
回复
1 回复

1,249 次查看
michaelestanley
NXP Employee
NXP Employee

Since you are only interested in vibrations, I recommend you take the vector magnitude of the accelerometer and operate on that.  You may also want to apply a high pass filter to remove gravity and low frequency accelerations.

0 项奖励
回复