Setting MMA8451 HPF

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Setting MMA8451 HPF

1,042 次查看
chrishedenberg
Contributor I

I'm trying set the high pass filter, and followed some of the instructions in the notes and using the arduino package already created. It works a bit, but when I lay the accelerometer flat I'm still getting some of the gravity effect (about half) in my data. I've tried to configure the settings to choose different cutoffs, but still no luck. I've seen that others on this site have nearly eliminated the effect of gravity. Here's a snapshot of my output and then my code taken, or adapted, from arduino code:

Output

         x,            y,            z
-1.29526,-4.54898, 1.33836
-1.29047,-4.54180, 1.31442
-1.29047,-4.54898, 1.30723

Set data rate to 2G with HPF default cutoff:

 uint8_t reg1 = readRegister8(MMA8451_REG_CTRL_REG1);
writeRegister8(MMA8451_REG_CTRL_REG1, 0x00); // deactivate
writeRegister8(MMA8451_REG_XYZ_DATA_CFG, 0b00001 & 0x13);
writeRegister8(MMA8451_REG_CTRL_REG1, reg1 | 0x01); // activate

Set data rate to 800Hz:

uint8_t ctl1 = readRegister8(MMA8451_REG_CTRL_REG1);
readRegister8(0x0F);
writeRegister8(MMA8451_REG_CTRL_REG1, 0x00); // deactivate
writeRegister8(0x0F, 0x00);
ctl1 &= ~(0b111 << 3); // mask off bits
ctl1 |= (0b000 << 3);
writeRegister8(MMA8451_REG_CTRL_REG1, ctl1 | 0x01); // activate

Set HPF:

uint8_t reg1 = readRegister8(MMA8451_REG_CTRL_REG1);
writeRegister8(MMA8451_REG_CTRL_REG1, 0x00); // deactivate
writeRegister8(MMA8451_REG_HPF, 0x03);
writeRegister8(MMA8451_REG_CTRL_REG1, reg1 | 0x01); // activate

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

831 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Chris,

In order to get the HPF data, the HPF_OUT bit must be set in the XYZ_DATA_CFG register (0x0E). Looking at your source code, you are not setting it correctly. You should use something like this:

 

writeRegister8(MMA8451_REG_XYZ_DATA_CFG, 0b000100XX);

 

where XX depends on the selected full-sacle range.

 

I hope it helps.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 项奖励
回复