Sensor MPX2300DT1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sensor MPX2300DT1

817 次查看
joergmeier
Contributor I

Is the Freescale Pressure Sensor MPX2300DT1 produced and packed under clean room conditions? Which class of cleanroom? Is the sensor sterilized after production? Do you have any document, that cerifies the cleanroom production?

0 项奖励
回复
1 回复

713 次查看
darioarias
NXP Employee
NXP Employee

Hello Joerg,

There is no documentation that certifies that the production of this part is made under clean room conditions and the part is no sterilized after production .This device have been designed with bio-medically approved materials with a history in medical situations to provide a sensor that can be used with confidence in applications, such as invasive blood pressure monitoring. It can be sterilized using ethylene oxide and it meets all USP XX Biological Testing Class VI requirements.

Darío

0 项奖励
回复