Seat angle sensor question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Seat angle sensor question

Jump to solution
2,106 Views
hyjung
Contributor II

Dear NXP engineer.

I'm looking for a device that senses the folded angle of the truck's seat back.

NXP has products from 2/3-axis sensor and angle sensor and wants to know which one is advantageous to use.

Can you briefly explain the typical device and why?

Thank you.

0 Kudos
Reply
1 Solution
2,005 Views
wtfan
NXP Employee
NXP Employee

Hello HY,

Thanks for your inquriy, this is Wenting from product line magnetic sensor marketing.

For the seat angle measurement application, it is imporant that you know it is a 2D measurement or 3D measurement that you are looking for.

2/3 axis sensor is based on MEMS technology and find application mostly in consumer or industry.

The 2D measurement magnetic sensor KMA family (KMA310, KMA321 or KMZ80) are sensors with different package most widely used in the Automotive industry. The sensor is doing nothing else than measuring a rotating magnetic field and convert the angle value to electrical signal, here our unique selling point is the accuracy and stability over life time, MR based technology is  in genenral more accurate against Hall based angle sensor. In case you are from South Korea, you might get in contact with Ms Sio Park for further support, she is our regional FAE in South Korea, Her contact  [email protected].

Regards,

Wenting

View solution in original post

0 Kudos
Reply
1 Reply
2,006 Views
wtfan
NXP Employee
NXP Employee

Hello HY,

Thanks for your inquriy, this is Wenting from product line magnetic sensor marketing.

For the seat angle measurement application, it is imporant that you know it is a 2D measurement or 3D measurement that you are looking for.

2/3 axis sensor is based on MEMS technology and find application mostly in consumer or industry.

The 2D measurement magnetic sensor KMA family (KMA310, KMA321 or KMZ80) are sensors with different package most widely used in the Automotive industry. The sensor is doing nothing else than measuring a rotating magnetic field and convert the angle value to electrical signal, here our unique selling point is the accuracy and stability over life time, MR based technology is  in genenral more accurate against Hall based angle sensor. In case you are from South Korea, you might get in contact with Ms Sio Park for further support, she is our regional FAE in South Korea, Her contact  [email protected].

Regards,

Wenting

0 Kudos
Reply