SPI write problems on an own reflown FXOS8700

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI write problems on an own reflown FXOS8700

5,296件の閲覧回数
hans-henrikfuxe
Contributor I

I have reflowed an FXOS8700 to my own development card as an breakout to be able to use it in a project. I am now unsure if it works proper or not.

Is the possibility to read but not write a sign of a burnt FXOS8700 in the reflow process????

SPI setting are CPOL=0 and CPHA=0:

I have no problem to read from an address, but problem to read back what was written.

This is my sequence of SPI commands:

    // WHO AM I
    SPI_ReadFXOS(WHO_AM_I, rbuf, 1);
    sprintf_P(buffer_0, PSTR("\r\n::WHO AM I = 0x%X\r\n\r\n"), rbuf[0]);
    uart_puts(buffer_0);

=> 0xC7

    // Temperature
    SPI_ReadFXOS(TEMP, rbuf, 1);
    sprintf_P(buffer_0, PSTR("\r\n::TEMP = %i\r\n\r\n"), rbuf[0]);
    uart_puts(buffer_0);

=> 21

Both above works as aspected!!!!

    // Acc + Mag TEST
    SPI_WriteFXOS(CTRL_REG1, 0x00);        // Set to standby mode
    SPI_ReadFXOS(CTRL_REG1, rbuf, 1);
    sprintf_P(buffer_0, PSTR("\r\n::CTRL_REG1 = 0x%X\r\n\r\n"), rbuf[0]);
    uart_puts(buffer_0);

    SPI_WriteFXOS(M_CTRL_REG1, 0x1F);    // 200 Hz hybrid mode
    SPI_ReadFXOS(M_CTRL_REG1, rbuf, 1);
    sprintf_P(buffer_0, PSTR("\r\n::M_CTRL_REG1 = 0x%X\r\n\r\n"), rbuf[0]);
    uart_puts(buffer_0);

=> 0x00

Writing to M_CTRL_REG1 does not work but gives 0x00 back ......

ラベル(2)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

4,980件の閲覧回数
hans-henrikfuxe
Contributor I

Now I have reflowed another two FXOS8700 vary carefully, and both of them show identical characteristics.

It is not possible to write to a register and than read it back, what can possible be wrong??

Write_and_read_M_CTRL_REG1.PNG

0 件の賞賛
返信

4,980件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Hans-Henrik,

It seems like your both write sequences are not correct. The order of the bits is as follows:

 

Byte 0: R/W, ADDR[6], ADDR[5], ADDR[4], ADDR[3], ADDR[2], ADDR[1], ADDR[0]

Byte 1: ADDR[7], X, X, X, X, X, X, X

Byte 2: DATA[7], DATA[6], DATA[5], DATA[4], DATA[3], DATA[2], DATA[1], DATA[0]

The first byte you are sending is correct, but the MSB bit of the second byte (ADDR[7]) should be "0" and not "1". So instead of sending 0xDB, 0xDB, 0x1F, try to send 0xDB, 0x00, 0x1F. Then send 0x5B, 0x00, 0x00 to read back 0x1F from the M_CTRL_REG1 register.

Hope it helps.

Best regards,

Tomas

4,980件の閲覧回数
hans-henrikfuxe
Contributor I

Thanks a bizillion times Tomas!

You are my hero and made my day, truly :smileyhappy:

I had used a macro (atmega8) in as if it returned the first bit as set, and it stayed to the second byte ...

Now all three modules work just fine!!!!

Best Regards,

Hans-Henrik

P.S: For anyone interested in atmega8 code looks like:

// Set FXOS8700 in SPI mode
void init_spi(void) {
    FXOS_SS_ENABLE;  // To open tri-state buffer and set MISO high
    MISO_HI;                    // SPI init demands SA0/MOSI high during reset
    FXOS_RESET_HI;     // Active high
    _delay_ms(1);             // ??
    FXOS_RESET_LO;
    _delay_ms(1);              // FXOS8700 Datasheet defines 1ms wait after reset [p.19]
    FXOS_SS_DISABLE;
}

// Read values from register FXOS8700
void SPI_ReadFXOS(uint8_t reg, volatile uint8_t* rbuf, uint8_t len) {

    FXOS_SS_ENABLE;

    ATOMIC_BLOCK(ATOMIC_RESTORESTATE) {
        SPDR = cbi(reg,7);                    // Transmit; clear bit 7 for reading + 7 bits of register address
        while(!(SPSR & 1<<SPIF));            // Wait for SPIF flag
        SPDR = reg;                            // Transmit bit 7 of register address
        while(!(SPSR & 1<<SPIF));            // Wait for SPIF flag

        for(uint8_t i=0; i<len; i++) {
            SPDR = 0x00;                    // Transmit
            while(!(SPSR & 1<<SPIF));        // Wait for SPIF flag
            rbuf[i] = SPDR;                    // Clear SPIF flag 2/2
        }
    }

    FXOS_SS_DISABLE;                // 2) For ISR context switcher which re-enable SPI unit
}

// Write value to register FXOS8700                                       <------------------------- ineffektiv loop
void SPI_WriteFXOS(uint8_t reg, uint8_t val) {

    FXOS_SS_ENABLE;

    uint8_t reg1 = reg;
    sbi(reg1,7);

    uint8_t wbuf[3] = {reg1, reg, val}; // Two bytes for write bit and address

    ATOMIC_BLOCK(ATOMIC_RESTORESTATE) {
        for(uint8_t i=0; i<3; i++) {
            SPDR = wbuf[i];                    // Transmit
            while(!(SPSR & 1<<SPIF));        // Wait for SPIF flag
        }
    }

    FXOS_SS_DISABLE;                // 2) For ISR context switcher which re-enable SPI unit
}

0 件の賞賛
返信

4,980件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Just for illustration, here is an example of writing/reading the value of 0x3D to/from the CTRL_REG1 (0x2A):

Write_Read.JPG

Best regards,

Tomas

0 件の賞賛
返信