S32K3 HVBMS RD Bring Up Example Build Problem | Code generation failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 HVBMS RD Bring Up Example Build Problem | Code generation failed

8,628 Views
shivchopra5
Contributor II

Hi,

I downloaded the HVBMS RD Bring UP Example.
I imported this project into S32DS.

I opened the .mex file and went to update the code. I received an "Code Generation failed" issue.
When I try to build main.c, it does not build, it is unable to find the files as seen in the output below.

I have the BMS SDK 0.9.0 and the BMS SDK SL 0.9.0 Demo libraries installed.
I also have the S32K3 RTD 2.0.0 installed.

Am I missing something when trying to build this project.
Thank you.

shivchopra5_0-1678398748145.pngshivchopra5_0-1678398748145.png

 

13:41:16 **** Incremental Build of configuration Debug_FLASH for project HVBMS-RD_Bring-up_example_S32DS ****
make -j8 all
Building file: ../src/Bjb.c
Building file: ../src/Cmu.c
Invoking: Standard S32DS C Compiler
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@src/Bjb.args" -MMD -MP -MF"src/Bjb.d" -MT"src/Bjb.o" -o "src/Bjb.o" "../src/Bjb.c"
Building file: ../src/Common.c
arm-none-eabi-gcc "@src/Bjb.args" -MMD -MP -MF"src/Cmu.d" -MT"src/Cmu.o" -o "src/Cmu.o" "../src/Cmu.c"
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@src/Bjb.args" -MMD -MP -MF"src/Common.d" -MT"src/Common.o" -o "src/Common.o" "../src/Common.c"
Building file: ../src/main.c
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@src/Bjb.args" -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.c"
../src/Bjb.c:26:10: fatal error: CDD_Bcc_772c.h: No such file or directory
26 | #include "CDD_Bcc_772c.h"
| ^~~~~~~~~~~~~~~~
compilation terminated.
../src/Cmu.c:26:10: fatal error: CDD_Bcc_775a.h: No such file or directory
Building file: ../generate/src/Clock_Ip_Cfg.c
26 | #include "CDD_Bcc_775a.h"
| ^~~~~~~~~~~~~~~~
compilation terminated.
make: *** [src/subdir.mk:29: src/Bjb.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [src/subdir.mk:29: src/Cmu.o] Error 1
Building file: ../board/Siul2_Port_Ip_Cfg.c
../src/Common.c:26:10: fatal error: Mcl.h: No such file or directory
26 | #include "Mcl.h"
| ^~~~~~~
compilation terminated.
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@generate/src/Clock_Ip_Cfg.args" -MMD -MP -MF"generate/src/Clock_Ip_Cfg.d" -MT"generate/src/Clock_Ip_Cfg.o" -o "generate/src/Clock_Ip_Cfg.o" "../generate/src/Clock_Ip_Cfg.c"
make: *** [src/subdir.mk:29: src/Common.o] Error 1
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@board/Siul2_Port_Ip_Cfg.args" -MMD -MP -MF"board/Siul2_Port_Ip_Cfg.d" -MT"board/Siul2_Port_Ip_Cfg.o" -o "board/Siul2_Port_Ip_Cfg.o" "../board/Siul2_Port_Ip_Cfg.c"
../src/main.c:26:10: fatal error: CDD_Bcc_775a.h: No such file or directory
26 | #include "CDD_Bcc_775a.h"
| ^~~~~~~~~~~~~~~~
compilation terminated.
make: *** [src/subdir.mk:29: src/main.o] Error 1
In file included from ../generate/src/Clock_Ip_Cfg.c:48:
C:/Users/Juan/Downloads/SW32K3_HVBMS-RD_Bring-up_Example_S32_DS_0_9_0_D2210/generate/include/Clock_Ip_Cfg.h:52:10: fatal error: Clock_Ip_Types.h: No such file or directory
52 | #include "Clock_Ip_Types.h"
| ^~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [generate/src/subdir.mk:20: generate/src/Clock_Ip_Cfg.o] Error 1
In file included from ../board/Siul2_Port_Ip_Cfg.c:43:
../board/Siul2_Port_Ip_Cfg.h:47:10: fatal error: Siul2_Port_Ip_Types.h: No such file or directory
47 | #include "Siul2_Port_Ip_Types.h"
| ^~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [board/subdir.mk:23: board/Siul2_Port_Ip_Cfg.o] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.

13:41:17 Build Failed. 13 errors, 0 warnings. (took 858ms)

0 Kudos
Reply
13 Replies

8,436 Views
shubhams21
Contributor I

Hello,

can anyone please provide link to download HVBMS Software Installation Guide?

 

Thank You!

 

0 Kudos
Reply

8,433 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Shubham,

As I mentioned below, the HVBMS Software Installation Guide is classified as a Secure File and can be downloaded from:

https://www.nxp.com/design/designs/hvbms-reference-design-bundle-using-etpl:RD-HVBMSCTBUN

Direct URL is:

https://www.nxp.com/webapp/sd/collateral/1669220275030722065315?version=2.0

Best regards,

Tomas

0 Kudos
Reply

8,371 Views
shubhams21
Contributor I

We got access to "HVBMS Software Installation Guide".

First step requires registration code, from we can get registration code?

0 Kudos
Reply

8,364 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Shubham,

The registration code is on the paper certificate that is shipped with the RD-HVBMSCTBUN.

Capture.JPGCapture.JPG

Best regards,

Tomas

0 Kudos
Reply

8,358 Views
shubhams21
Contributor I

Thank You for the response.

One more question, the HVBMS we received is preflashed with firmware version 0.8.0, so where can I get compatible HVBMS_StartUp_FreeMASTER.elf file?

0 Kudos
Reply

8,348 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Shubham,

We strongly recommend to upgrade the FW with the latest .elf file (firmware 0.9.1) and use the latest HVBMS Start-up Interface.

Capture.JPGCapture.JPG

Both can be downloaded from:

https://www.nxp.com/design/designs/hvbms-reference-design-bundle-using-etpl:RD-HVBMSCTBUN

SW.JPGSW.JPG

Best regards,

Tomas

0 Kudos
Reply

8,095 Views
shubhams21
Contributor I
can we use "SEGGER J-Link EDU Mini" debugger to upgrade the firmware version to 0.9.1 ?
0 Kudos
Reply

8,284 Views
shubhams21
Contributor I

Hello Tomas,

We don't have PE Micro debugger with us to Flash firmware version 0.9.1

1. We have IAR I-JET debugger, can we use that?

2. We have S32K144 EVB Q-100 board, and it has on board debugger, can we use that to flash firmware on RD-K344BMU?

 

Best regards,

Shubham

0 Kudos
Reply

8,276 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @shubhams21,

The OpenSDA debugger on that board is a PEMicro proprietary debugger.

Please have a look at the Getting Started with the S32K144EVB document:

https://www.nxp.com/document/guide/getting-started-with-the-s32k144evb:NGS-S32K144EVB?section=build-...

 

Regards,

Daniel

0 Kudos
Reply

8,256 Views
shubhams21
Contributor I

shubhams21_0-1681468866059.pngshubhams21_0-1681468866059.png

We are trying to Flash firmware to RD-K344BMU, getting this error.

Could you please help us?

 

0 Kudos
Reply

8,600 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Shiv,

I have asked our HVBMS SW expert to help with the software issue you are facing. He is currently on sick leave, but should be able to answer at the beginning of next week.

Thank you in advance for your patience.

Best regards,

Tomas

0 Kudos
Reply

8,563 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Shiv,

First of all, please make sure you have all the packages installed in the right order, presented in section 5.1.1 of the HVBMS Installation Guide. This is really important, even some colleagues faced similar problems when they did not follow the order. 

Capture.JPGCapture.JPG

There can be multiple reasons for the failure, here is a list:

1. Installation order from the HVBMS installation guide was not followed, BMS SDK was installed first then RTD.
2. Generation timeout of S32DS in order to fix this issue see section : 5.1.1.8.3.1 form the HVBMS installation guide.

“In case of difficulties in the code generation using S32 Configuration due to computer speed, it is possible to remove the timeout in the C:\NXP\S32DS.3.4\eclipse\s32ds.ini file by adding the following line: -Dcom.nxp.swtools.codegenscript.timeout=-1.”

After adding this in .ini file please restart S32DS and create a new workspace where a fresh import has to be tried.

I hope it helps!

Best regards,

Tomas

PS: The HVBMS Installation Guide is classified as a Secure File and can be downloaded from the following website:

https://www.nxp.com/design/designs/hvbms-reference-design-bundle-using-etpl:RD-HVBMSCTBUN

Capture 1.JPGCapture 1.JPG

 

0 Kudos
Reply

8,546 Views
shivchopra5
Contributor II

Thanks, I didn't know about the HVBMS Software Installation Guide
I will follow the guide and update the ticket.

Thank you!

0 Kudos
Reply