S12DP512 interface with 3.3V devices.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S12DP512 interface with 3.3V devices.

1,971 次查看
monstor
Contributor II

Dear all,

I want to use S12DP512 to interface with a pressure sensor and accelerometer.

The voltage of these sensors Vdd are 3.3V and the Vdd of S12DP512 is 5V.

How can the MCU interface with these sensors? Should I need a level shifter? or They are TTL compatible?

Thanks for your helping.

标签 (1)
标记 (3)
0 项奖励
回复
5 回复数

1,708 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Henry,

You did not specify which sensors you are going to use, but in general I would suggest using both a logic level converter and a 3.3V regulator to allow everything to run at the proper voltages.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

1,708 次查看
monstor
Contributor II

Dear Tomas,

I would like to connect to 3 I2C sensors. 1 of them is 5.5Vdc max. so

there is no problem of it. The others are 3.6Vdc max.

They are :

1. Freescale FXLS8471Q (Linear Accelerometer)

2. Measurement Specialties MS5607-02BA03 (Barometric Pressure Sensor)

I cannot confirm are they TTL compatible. If yes, I think I don't need a

level shifter IC. Do you have any recommendation?

Really thanks for your helping.

Best regards,

Henry

0 项奖励
回复

1,708 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Henry,

Pulling the bus to 5V is not really a solution since both the SDA and SCL pins are not tolerant of voltages higher than VDDIO + 0.3V (3.6V max).

However, looking at the MC9S12DP512 specs, the minimum voltage for a high level is 0.65*Vdd, which is 3.25V at a 5V supply. So, if you pull the I2C bus to 3.3V, you might not need an I2C level shifter.


Regards,

Tomas

0 项奖励
回复

1,708 次查看
monstor
Contributor II

Dear Tomas,

Thanks for your reply.

I can understand your theory. That mean MCU side can accept the high

signal from sensor once the voltage level is higher than 3.25V.

However, can the sensor accept the high signal from the MCU? The VDD of

the sensor is 3.6V max.

Best regards,

Henry

0 项奖励
回复

1,708 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Henry,

I do not quite understand what you mean by „can the sensor accept the high signal from the MCU“. The trick is to connect the pull-up resistors to the lower of the two voltages, in our case to 3.3V. When the output transistor is off, the resistor connects the pin to 3.3V (not to 5V).


Regards,

Tomas

0 项奖励
回复