Receiver module for FXTH87XXX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Receiver module for FXTH87XXX

1,747 次查看
lithinreddymarl
Contributor I

Hello! I am working on TPMS for a commercial vehicle and looking for a receiver compatible with FXTH870511DT1 sensor(which has integrated Tx).

Any help in finding the sensor will be of great help.

标记 (2)
3 回复数

1,548 次查看
franklatona-r49
NXP Employee
NXP Employee

Hello Maria,

Freescale does have a transceiver that supports full RX/TX functionality in the sub-GHz space (290-340 MHz, 424-510 MHz, and 862-1020 MHz frequency bands):

KW0x |Kinetis KW0x Sub-1 GHz Radio MCUs|Freescale

In addition there is an application note in its final stages using the MKW01 as the receiver for the FXTH870xD TPMS Sensor which I can forward to you when it completed.  Please send me an email directly at frank.latona@freescale.com for this.

Thank you for interest in Freescale TPMS Solutions.

Frank

1,548 次查看
lithinreddymarl
Contributor I

Hello Frank,

Thanks a lot for the help. Isn't MKW01Z128 transceiver an industrial grade product? I am looking for an automotive grade receiver for the sensor.Can u please suggest an effective replacement for MKW01Z128?

Thank you!

0 项奖励
回复

1,548 次查看
michaelestanley
NXP Employee
NXP Employee

Hi Maria.  This portion of the community targets sensor fusion topics.  So the TPMS support engineers may have missed it.  I'll ask them to log in and reply.