RISC-V EDUCATION

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,835件の閲覧回数
CYBORGJ
Contributor I

IS THERE AN NEED FOR EDUCATION IN USING RISC-V  ISA  FOR SENSORS AND SOFTWARE REQUIREMENTS WITH THE POSSIBILITY OF NO FIRST ERROR? A TECHNIQUE?

0 件の賞賛
返信
1 解決策
2,816件の閲覧回数
CYBORGJ
Contributor I

Hi,

since once I spent 8 hours developing a C program for a Texas Instruments launchpad that used SPI communication (which can be very intricate) I was successful. After that I realized the process can be standardized into a type of secretarial work procedure using a 3 step process which can then be used to create a no first error program to meet Software Requirements. Since some of the MEMS  are very useful, my process may be be a needed one?

 

Thus, my process may be applicable to many different type of mems as I only used it for a specific  3-axis magnetic MEMS.

 

John

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,831件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Which part do you mean for this topic?


0 件の賞賛
返信
2,817件の閲覧回数
CYBORGJ
Contributor I

Hi,

since once I spent 8 hours developing a C program for a Texas Instruments launchpad that used SPI communication (which can be very intricate) I was successful. After that I realized the process can be standardized into a type of secretarial work procedure using a 3 step process which can then be used to create a no first error program to meet Software Requirements. Since some of the MEMS  are very useful, my process may be be a needed one?

 

Thus, my process may be applicable to many different type of mems as I only used it for a specific  3-axis magnetic MEMS.

 

John

0 件の賞賛
返信