Purpose of Stainless Steel cover on MPX5999D

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Purpose of Stainless Steel cover on MPX5999D

ソリューションへジャンプ
1,324件の閲覧回数
awolfe1
Contributor I

I assume the stainless steel cover on the MPX5999D is to protect the internal component of the pressure transducer.  I also assume it has no structural purpose when the transducer is under pressure, is that correct?

I am asking because we would like to add a compatible gel to the transducer before installing the transducer behind a movable diaphragm, and have found that removing the plate makes it easier to add the gel without air being trapped in the assembly.  I am sure that you could not recommend or warrant this process as we are modifying your original assembly, but if you could simply answer the question above it would be helpful to us.

0 件の賞賛
返信
1 解決策
1,242件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Aaron,

You are correct. The stainless steel lid is for mechanical protection and does not influence the performance of the sensor itself (other than the hole in the lid to allow air to vent).

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,242件の閲覧回数
awolfe1
Contributor I

A follow up question... what kind of volume would we need to buy in order to purchase transducers without the stainless steel lid?  Is it even possible?

Thank you,

Aaron

0 件の賞賛
返信
1,243件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Aaron,

You are correct. The stainless steel lid is for mechanical protection and does not influence the performance of the sensor itself (other than the hole in the lid to allow air to vent).

Best regards,

Tomas

0 件の賞賛
返信