NTM88 maximum sensor samples per second via SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NTM88 maximum sensor samples per second via SPI

3,081 次查看
martijn-VB
Contributor I

Hello,

We're interested in using the NTM88 in one of our applications.

What is the maximum samples per second we can get from the pressure sensor and accelerometer? And what is the maximum response time of both sensors? (I couldn't find it in the datasheet, I might have overlooked it...)

With kind regards,
Martijn

标签 (1)
0 项奖励
回复
5 回复数

2,855 次查看
martijn-VB
Contributor I

Can anyone point me in the right direction?
I'm not looking for SPI information but information about the actual sensing elements in the chip.

How fast is the pressure sensor and accelerometer?
Does the pressure and accelero reading from the sensor update with 1Hz or with 1000Hz?

And what is the reponsetime of the sensors?
If the pressure or accelerration in the vehicle change very fast (ms range), how fast will the sensor reading out of the sensor change?

0 项奖励
回复

2,829 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Sorry for not responding earlier.

Please see Implementing Wired Communication with the NTM88 

 

0 项奖励
回复

3,001 次查看
martijn-VB
Contributor I

Hi ErikaC,

I'm sorry, I've not formulated my question clear enough.
I was not looking for the SPI specific information but sensor specific.

How fast is the pressure sensor and accelerometer?
Does the pressure and accelero reading from the sensor update with 1Hz or with 1000Hz?

And what is the reponsetime of the sensors?
If the pressure or accelerration in the vehicle change very fast (ms range), how fast will the sensor reading out of the sensor change?

With kind regards,
Martijn

0 项奖励
回复

2,954 次查看
martijn-VB
Contributor I

@ErikaCAny more information on this?

0 项奖励
回复

3,052 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello, please refer to the SPI section of the NTM88 manual for information on the protocol and frame format supported by the NTM88 UM11227 section 10.18, and the attached document.

Hope this helps.

 

 

0 项奖励
回复