NTM88 flash address 0xfd40~0xfdff cannot be programmed.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTM88 flash address 0xfd40~0xfdff cannot be programmed.

1,071 Views
tedwu1
Contributor III

Hi I used NTM88 for TPMS project. Now, I cannot program data into address between 0xfd40~0xfdff. I knew them are form parameter and I backup them. They are 0xBA between 0xfd40~0xfdff. And 0xffb0~fff7 are 0xff. 0xffb8 ~0xffbf are 0xba,0xba,0xba,0xba,0xba,0xff,0xba,0x82. How to re-write parameter into address of 0xfd40~0xfdff?

0 Kudos
Reply
1 Reply

1,054 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Ted,

Please keep in mind that trim coefficients are programmed between 0xFD40 and 0xFDFF (see the AN12524 for more information).

Capture.JPG

The trim coefficients are unique to each device and they must not be erased or overwritten, otherwise the sensor measurements will be out-of-range.

In CodeWarrior, the NTM88_LIB patch prevents the CW programming tool to erase these coefficients, that is why they are never erased nor overwritten by CW even if they are referenced in the s19 file.

Best regards,

Tomas

0 Kudos
Reply