Magnetometer Development Board does not startup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Magnetometer Development Board does not startup

跳至解决方案
1,889 次查看
frankbenkert
Contributor I

Dear community,

I followed the steps described in the Quick Start Guide:

* Download Software from freescale.com\sensortoolbox

* Installed Software - no Errors occured

* Connected Evalboard to USB-port and switched the power Switch to on (red led is on)

* FTDI-Driver is installed (checked in Device Manager)

* Software started

and then it appears a window "Loading Freedom Sensor Toolbox(CE) - Please wait..." and nothing happens

Can anybody help?

Thanks

Frank

1 解答
1,481 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Frank,

Could you please specify which development board are you using? If it is the RD4247MAG3110 (LFSTBEB3110), please download and install the E-Compass Sensor Toolbox v6.1.0.1.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

在原帖中查看解决方案

3 回复数
1,481 次查看
shuaizhang
Contributor I

I can not download  the E-Compass Sensor Toolbox v6.1.0.1, it say Page Not Found

can you sent it to my email 364023214@qq.com .thanks very much. i really need it now. I'm looking forward to your reply.

0 项奖励
回复
1,482 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Frank,

Could you please specify which development board are you using? If it is the RD4247MAG3110 (LFSTBEB3110), please download and install the E-Compass Sensor Toolbox v6.1.0.1.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

1,481 次查看
frankbenkert
Contributor I

Dear Tomas,

yes, indeed it is the LFSTBEB3110 Magnetometer Development Board. With your help and downloading the E-Compass Sensor Toolbox it works now.

Maybe it is worth thinking about adding this Detail to the Quick Start Guide.

Nevertheless Thanx for your quick Response.

Regards

Frank

0 项奖励
回复