MPXV5100 and negative pressure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPXV5100 and negative pressure

996件の閲覧回数
Houarcheneger
Contributor I

Dear all,

I know MPXV5100 only works with positive pressure, however I would like to know what if a depressure is applied. Does the membrane break out? If yes, what is the critical pressure?

Thanks for your help.

Nicolas.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

792件の閲覧回数
darioarias
NXP Employee
NXP Employee

You are correct, because in a gauge pressure sensor, P2 is open to the ambient (1 atm, always). If P1 is negative pressure (less than 1 atm) or vacuum, then P2 > P1, which breaks the condition to keep the integrity of the sensor. If you want to measure negative pressure, my advice would be to get a differential pressure sensor.

Darío

0 件の賞賛
返信

792件の閲覧回数
Houarcheneger
Contributor I

Thank you very much for your answer!

I did not tell it but my MPXV5100 isthe GP one, so there is no second port, thus a negative pressure would damage my device...

Nicolas.

0 件の賞賛
返信

792件の閲覧回数
darioarias
NXP Employee
NXP Employee

Hi Nicolas,

The MPX5100DP will not be damaged as long as the pressure in port one is greater than pressure in port two (P1>P2). Hence if you apply depressure, the device will be fine, as long this pressure is applied to the Port 2.

Dario

0 件の賞賛
返信