Hi,
I have a MPX5010DP pressure sensor connected to an Arduino Uno.
Pin 1 (with the mark) on the MPX5010DP is connected to Pin A0, Pin 2 is connected to Ground and Pin 3 to 5V on the Arduino.
Without any pressure applied, the offset value is about 1.58 V.
The sensitivity is about 2.43 mV/mm H2O. These values does not match the datasheet values : 0.2 V for the offset, 4.413 mV/mm H2O for the sensitivity.
I can't see anything wrong with my setup.
Has anyone ever observed this kind of problem?
Thanks
已解决! 转到解答。
Hello,
These devices are very sensitive. To ensure optimal performance, we recommend implementing auto-zero according to the application note linked below:
Implementing Auto-Zero for Integrated Pressure Sensors
Hope this helps.
Hello,
These devices are very sensitive. To ensure optimal performance, we recommend implementing auto-zero according to the application note linked below:
Implementing Auto-Zero for Integrated Pressure Sensors
Hope this helps.