Hi
For medical applications, the use of silicone oil (liquid) for pressure conduction is used to measure the height difference between point A and point B. Currently we have tried many types of silicone oil, which can damage the sensor and no longer work, but we have also seen other similar products used. The liquid is not water, but we don't know what it is, it has a density of 0.9. I was wondering if there are any recommended liquids, thanks.
best regards
解決済! 解決策の投稿を見る。
Hi Joe,
I do fully understand your question.
What I can say about the MPX2300DT1 is that the gel coating is on the backside of the device where a little nose is:
Attached you can find the documentation for both the gel, opaque filler and molding compound. The pigment id Ferro 61-88450. It is mixed 4% with the Dow Corning 7-9600 gel.
BR, Tomas
Hi Joe,
I do fully understand your question.
What I can say about the MPX2300DT1 is that the gel coating is on the backside of the device where a little nose is:
Attached you can find the documentation for both the gel, opaque filler and molding compound. The pigment id Ferro 61-88450. It is mixed 4% with the Dow Corning 7-9600 gel.
BR, Tomas
Hi TomasVakerka,
Are there any recommended liquid media for medical applications, or have there been any successful cases of similar customers? Thank you very much.
best regards,
Joe