MPX2202A / MPX599D wiring problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPX2202A / MPX599D wiring problem

ソリューションへジャンプ
1,152件の閲覧回数
lucas_s
Contributor I

Hi,

I bought MPX2202A Si Pressure Sensor in case 344-15. I have a big problem with connecting it properly as on p.8 of datasheet there are three styles of connection, which are very different from each other. Which style I should use? Same question about MPX5999D in case 867? Thank you in advance.

ラベル(1)
0 件の賞賛
返信
1 解決策
963件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Lucas,

The MPX2202A is a compensated pressure sensor with a differential output (+Vout and -Vout), so the pin description is as follows:

1 – GND

2 – +Vout

3 – Vs

4 – -Vout

The MPX599A is a fully integrated pressure sensor with a single ended output:

1 – Vout

2 – GND

3 – Vs

4 – V1

5 – V2

6 – VEX

V1, V2 and VEX pins are used for factory trimming and then they are laser cut. We recommend to leave these pins floating.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

元の投稿で解決策を見る

2 返答(返信)
963件の閲覧回数
lucas_s
Contributor I

Hi Tomas,

thank you very much, that was quick and accurate answer!

Kind regards, Lucas.

0 件の賞賛
返信
964件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Lucas,

The MPX2202A is a compensated pressure sensor with a differential output (+Vout and -Vout), so the pin description is as follows:

1 – GND

2 – +Vout

3 – Vs

4 – -Vout

The MPX599A is a fully integrated pressure sensor with a single ended output:

1 – Vout

2 – GND

3 – Vs

4 – V1

5 – V2

6 – VEX

V1, V2 and VEX pins are used for factory trimming and then they are laser cut. We recommend to leave these pins floating.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.