MPR083 Demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,102件の閲覧回数
grahambaker
Contributor I

How do I connect the MPR083 to my computer? Do I need an downloads for it other than the Sensor Toolbox?

0 件の賞賛
返信
1 解決策
2,028件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Graham,

The KITMPR083EVM does not belong to the Sensor Toolbox tools. There is a specific PC application (PC_GUI_KITMPR08X) for this board available either on the CD that comes along with the kit or on this website.

As a side note, both the MPR083 and KITMPR083EVM are EOL, I would recommend to go over to the MPR121 if you want to continue having this sort of function.

I hope this helps.

Regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,029件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Graham,

The KITMPR083EVM does not belong to the Sensor Toolbox tools. There is a specific PC application (PC_GUI_KITMPR08X) for this board available either on the CD that comes along with the kit or on this website.

As a side note, both the MPR083 and KITMPR083EVM are EOL, I would recommend to go over to the MPR121 if you want to continue having this sort of function.

I hope this helps.

Regards,

Tomas

0 件の賞賛
返信