MPR03x pad shape/area

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPR03x pad shape/area

跳至解决方案
4,020 次查看
onechil
Contributor II

The app. note in the link below suggests suggests that "The minimum pad size for Freescale’s products is 3 mm by 3 mm when using thin film overlays to about 0.5 mm thickness of acrylic or ABS plastic".

In a proximity sensing application, assuming the area of the object to be sensed is >= 9mm sq. and the profile of the object is planar to the sensing electrode pad on a PCB, is it accurate to interpret the 3mm x 3mm recommendation, as a 9mm sq. minimum electrode pad area for Freescale's touch sensing products?

Thanks,

标签 (1)
1 解答
3,681 次查看
Joshevelle
Senior Contributor I

Hello onechil,

Yes.

Proximity sensors like the MPR03x sense changes in the Electrode Capacitance, which is related to the electrode's area. We suggest a minimum of 3x3mm which equals to 9mm sq area. So yes, you shouldn't have any issues.

Hope it helps.

Josh

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,682 次查看
Joshevelle
Senior Contributor I

Hello onechil,

Yes.

Proximity sensors like the MPR03x sense changes in the Electrode Capacitance, which is related to the electrode's area. We suggest a minimum of 3x3mm which equals to 9mm sq area. So yes, you shouldn't have any issues.

Hope it helps.

Josh

0 项奖励
回复
3,681 次查看
onechil
Contributor II

Hi Joshevelle,

Sounds good! I thought as much, but wanted some clarification, cheers.

3,681 次查看
Joshevelle
Senior Contributor I

You're welcome. Have fun!

Josh

0 项奖励
回复
3,681 次查看
onechil
Contributor II

Actually I have one more question - I haven't been able to find a recommended PCB footprint for the MPR03x uDFN part. Would you be able to refer me to one? Thanks.

0 项奖励
回复