MPR031 HELP!!!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPR031 HELP!!!

2,284 次查看
rfslf
Contributor I

Please help me!
I use MPR031, and I can not start-up.

When I send 0x4A address, line is tied to ground and I cannot send command address.
When I send address from all range of possible, MPR031 does not respond.
MPR031 soldered well, contact is good. There is no answer from MPR031.

Please help me examples of an initial configuration of registers for MPR031.

 


Best regards,
Alex

0 项奖励
回复
2 回复数

1,782 次查看
leo_oto
Contributor I

Did it work? I have the same problem. But it responds the adress but gets all zeros from EVERY register. Even if i write before i read. 

0 项奖励
回复

1,782 次查看
TomE
Specialist II

> I have the same problem. But it responds the adress..

 

Which is not the same problem. The original poster couldn't get a response at all.

 

Have you read the other posts in this forum on the MPR031 (and MPR121)?

 

Type "MPR031" into the Search Box and read the previous articles.

 

Tom

 

0 项奖励
回复