MPL3115A2, I2C pull up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPL3115A2, I2C pull up

1,752 Views
owlowner
Contributor I

MPL3115A2,Dose I2C need an external pull up voltage?or it has been pulled up inside by VDDIO?And can you give an advise for pull up resistance?

Labels (1)
0 Kudos
Reply
3 Replies

1,507 Views
shubhadippaul-b
NXP Employee
NXP Employee

Yes, external pull ups should be applied to I2C lines for MPL3115. Suggested value is 4.7k.

Please refer to FRDMSTBC-P3115-SCH for a reference connection setup of MPL3115.

0 Kudos
Reply

1,507 Views
owlowner
Contributor I

Ok ,thank you。 What the function of VDDIO?

0 Kudos
Reply

1,507 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Polo,

VDD is the main power supply for all internal analog and digital functional blocks.

 

VDDIO is a separate power supply pin used for the supply of the I2C digital communication interface.

 

So VDDIO sets the interface voltage level for the MPL3115A2 and your MCU. For single-supply operation, VDDIO can be the same as the main supply VDD. In a dual-supply applications, however, VDDIO can differ from VDD to accommodate the desired interface voltage.

Let us know if you have any other questions.

Best regards,

Tomas

0 Kudos
Reply