MPL3115A2, I2C pull up

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPL3115A2, I2C pull up

1,913 次查看
owlowner
Contributor I

MPL3115A2,Dose I2C need an external pull up voltage?or it has been pulled up inside by VDDIO?And can you give an advise for pull up resistance?

标签 (1)
0 项奖励
回复
3 回复数

1,668 次查看
shubhadippaul-b
NXP Employee
NXP Employee

Yes, external pull ups should be applied to I2C lines for MPL3115. Suggested value is 4.7k.

Please refer to FRDMSTBC-P3115-SCH for a reference connection setup of MPL3115.

0 项奖励
回复

1,668 次查看
owlowner
Contributor I

Ok ,thank you。 What the function of VDDIO?

0 项奖励
回复

1,668 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Polo,

VDD is the main power supply for all internal analog and digital functional blocks.

 

VDDIO is a separate power supply pin used for the supply of the I2C digital communication interface.

 

So VDDIO sets the interface voltage level for the MPL3115A2 and your MCU. For single-supply operation, VDDIO can be the same as the main supply VDD. In a dual-supply applications, however, VDDIO can differ from VDD to accommodate the desired interface voltage.

Let us know if you have any other questions.

Best regards,

Tomas

0 项奖励
回复