MMA8652 : Using on highlands

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA8652 : Using on highlands

Jump to solution
2,377 Views
koichisakagami
Contributor II

Dear community,
We have been developing our product with MMA8652.

We hope to use the MMA8652 on Low pressure environment ( 472mbar ) .

A 472mbar is equivalent to altitude degree of 6000m.

[Question]
   Are there any problem using in such a environment ?

   We could not find a note in MMA8652 data sheet.

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
1 Solution
2,205 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Koichi Sakagami,

We don’t have any evaluation done at such low pressure environment.

But, according to our chief engineer, since the g-cell is hermetically sealed at the bond pressure it is not affected by the ambient pressure changes. So, operating at a lower pressure should not affect the pressure in the g-cell and therefore will not affect the performance.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
2,205 Views
koichisakagami
Contributor II

Dear Jose,

Thank you for your information.

We will study them.

Best Regards,

Koichi Sakagami

0 Kudos
2,206 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Koichi Sakagami,

We don’t have any evaluation done at such low pressure environment.

But, according to our chief engineer, since the g-cell is hermetically sealed at the bond pressure it is not affected by the ambient pressure changes. So, operating at a lower pressure should not affect the pressure in the g-cell and therefore will not affect the performance.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos