MMA8451Q interrupt read mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA8451Q interrupt read mode

1,310 Views
maurogatti
Contributor I

Hello.

I configured the MMA8451Q with ODR = 800Hz, so I can read the acceleration's components with a 1,25 ms  sample period.

The  polling mode is ok, I can do a read with  800Hz sample frequency.

But I can do it in "interrupt mode" (I configured MMA8551 as described in AN4076) because I see the interrupt pulse every 24 ms (about 40 Hz).

Why? 

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,043 Views
david_diaz
NXP Employee
NXP Employee

Hello Mauro,

Thank you very much for writing.

In this case, I highly recommend to use the sample project from the link below as a reference for your application:

https://community.nxp.com/docs/DOC-98836 

Please note that in the project, the interrupt mode is used.

Please let me know if you have any further question and I will be glad to help you.

 

Best Regards,

David

0 Kudos
Reply