Linux Driver of MMA8451Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux Driver of MMA8451Q

2,031件の閲覧回数
xianianjiong
Contributor I

I want to MMA8451Q in our product.

Current product platform is Ti DM355 (linux2.6.10)

Developing product platform is Ti DM368 (linux 2.6.32)

Where i can get the linux dirver code of MMA8451Q

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,561件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Xia,

You can download the MMA845x full-feature driver based on Linux 2.6.35 kernel source code from the following website:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=SNSDRVSANDROID&nodeId=0152109D3F&fpsp...


I hope it helps.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 件の賞賛
返信

1,561件の閲覧回数
xianianjiong
Contributor I

Hi,

Thanks.

I will try it on our platform.

Nianjiong.Xia(夏年炯) | Firmware Engineer

Dental/R&D

xia.nianjiong@carestreamhealth.com

Office: 8621 3852 6445 Fax: 8621 5834 5818

www.carestreamhealth.com

Carestream Health | Bldg 10, Jinqiao Software Park, No 27 Xin Jinqiao Rd |

Shanghai, China

上海市新金桥路27号金桥软件园10号楼锐珂(上海)医疗器材有限公司

201206

0 件の賞賛
返信