KTY84-130 replacement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KTY84-130 replacement

4,115件の閲覧回数
rachelwang
Contributor I

Is KTY84-130 going to be phased out?  I'm looking for the possible replacement of it.  What' s the type of the replacement?  Thanks!

0 件の賞賛
返信
1 返信

2,889件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Rachel,

Indeed, the KTY84-130’s status is End of life, which means that the capacity is declining rapidly. Formal discontinuance notice may be issued.

In this case I would like to recommend the KTY81: Silicon temperature sensors.

The temperature sensors in the KTY81 series have a positive temperature coefficient of resistance and are suitable for use in measurement and control systems. The sensors are encapsulated in the SOD70 2 in-line leads plastic package.

sensor.jpg

You may find more information here​.

Please let me know if this recommendation is useful for you.

If I misunderstood your question, feel free to let me know.  I will be glad to help.

Have a great day.

David Diaz.

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛
返信