KMI25/4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
2,617 次查看
UliHoss
Contributor I

What is the meaning of "Z" in the order information of the KMI25/4Z ???

There was a former part with ordering number KMI25/4X which is not longer manufactured, but there is no description what the meaning of the ending is (Z or X)

0 项奖励
回复
1 解答
2,594 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Uli,

The only difference is in the packing method.

KMI25/4Z: REEL-Reel 13" Q4/T2

KMI25/4X: REEL-Reel 7" Q1/T1

BR, Tomas

在原帖中查看解决方案

2 回复数
2,584 次查看
UliHoss
Contributor I

Great, thank you Tomas

0 项奖励
回复
2,595 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Uli,

The only difference is in the packing method.

KMI25/4Z: REEL-Reel 13" Q4/T2

KMI25/4X: REEL-Reel 7" Q1/T1

BR, Tomas