KMI25/4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
2,606 Views
UliHoss
Contributor I

What is the meaning of "Z" in the order information of the KMI25/4Z ???

There was a former part with ordering number KMI25/4X which is not longer manufactured, but there is no description what the meaning of the ending is (Z or X)

0 Kudos
Reply
1 Solution
2,583 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Uli,

The only difference is in the packing method.

KMI25/4Z: REEL-Reel 13" Q4/T2

KMI25/4X: REEL-Reel 7" Q1/T1

BR, Tomas

View solution in original post

2 Replies
2,573 Views
UliHoss
Contributor I

Great, thank you Tomas

0 Kudos
Reply
2,584 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Uli,

The only difference is in the packing method.

KMI25/4Z: REEL-Reel 13" Q4/T2

KMI25/4X: REEL-Reel 7" Q1/T1

BR, Tomas