KMI25/4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,602件の閲覧回数
UliHoss
Contributor I

What is the meaning of "Z" in the order information of the KMI25/4Z ???

There was a former part with ordering number KMI25/4X which is not longer manufactured, but there is no description what the meaning of the ending is (Z or X)

0 件の賞賛
返信
1 解決策
2,579件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Uli,

The only difference is in the packing method.

KMI25/4Z: REEL-Reel 13" Q4/T2

KMI25/4X: REEL-Reel 7" Q1/T1

BR, Tomas

元の投稿で解決策を見る

2 返答(返信)
2,569件の閲覧回数
UliHoss
Contributor I

Great, thank you Tomas

0 件の賞賛
返信
2,580件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Uli,

The only difference is in the packing method.

KMI25/4Z: REEL-Reel 13" Q4/T2

KMI25/4X: REEL-Reel 7" Q1/T1

BR, Tomas