KITMPR121EVM MPR121 Touch Sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KITMPR121EVM MPR121 Touch Sensor

ソリューションへジャンプ
1,543件の閲覧回数
grahambaker
Contributor I

I purchased the KITMPR121EVM MPR121 Touch Sensor Kit. I downloaded the Sensor Toolbox, but it appears that this is only for evaluation. What do I use for software development with the MPR121 Sensor?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,231件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Graham,

You are right, the Sensor Toolbox has been primarily designed to easily evaluate our sensors without any programming.

If you are looking for hardware and software to support product prototyping efforts, I would rather recommend using the TWR-SENSOR-PAK module that contains among others the MPR121 plug-in module (TWRPI-MPR121). The source code, schematic as well as the CodeWarrior for Microcontrollers v6.3 are accessible here. There is also available the User Manual.

I hope it helps.

Regards,

Tomas 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,232件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Graham,

You are right, the Sensor Toolbox has been primarily designed to easily evaluate our sensors without any programming.

If you are looking for hardware and software to support product prototyping efforts, I would rather recommend using the TWR-SENSOR-PAK module that contains among others the MPR121 plug-in module (TWRPI-MPR121). The source code, schematic as well as the CodeWarrior for Microcontrollers v6.3 are accessible here. There is also available the User Manual.

I hope it helps.

Regards,

Tomas 

0 件の賞賛
返信