Issue with STB v6.1.0.2 with MAG3110 Magnetometer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with STB v6.1.0.2 with MAG3110 Magnetometer

1,864 Views
wiliamlang
Contributor I

I am trying to run the Sensor Toolbox with the MAG3110 daughter card.  When I select the "eCompass" tab, I get an unhandled exception - "Could not load file or assembly 'National Instruments.Common.Version=9.1.40.159 ...'.  I've attached an image of the full error message.  I've tried this on two separate machines and get the same error.  The first is running Windows 7 Professional 64bit Service Pack 1.  The second is Windows XP 32bit Service Pack 3.  Any help would be appreciated.  Thank you.

Labels (2)
0 Kudos
Reply
2 Replies

1,547 Views
wiliamlang
Contributor I

I found the answer elsewhere on this site: Re: LFSTBEB3110 troubleshooting .  I downloaded and installed v6.1.0.1 and it seems to work.  In fact, both v6.1.0.1 and v6.1.0 2 work now.

0 Kudos
Reply

1,547 Views
anthonyduhamel
NXP Employee
NXP Employee

Thanks for your feedback William!

0 Kudos
Reply