Is there any document about power cycling of a gyroscope of NXP? Specifically, i am interested in a current consumption profile (or model) for single sample method!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any document about power cycling of a gyroscope of NXP? Specifically, i am interested in a current consumption profile (or model) for single sample method!

855 Views
giovannischibon
Contributor I

Ideally i would like to have a odcumentation like the one from paper "Achieving Lowest Power Consumption with MMA8491Q Accelerometer/Tilt Sensor".

0 Kudos
Reply
1 Reply

787 Views
david_diaz
NXP Employee
NXP Employee

Hello Giovanni,

Unfortunately, there is no such document.

The FXAS21002C is a low power device. The current consumption in Active mode is 2.7 mA.

In this case, I would recommend to transit from Active to Ready mode when no measurements are being made. This mode offers the user the ability to significantly reduce the current draw of the device while providing a fast transition into Active mode within 1/ODR + 5ms.

I hope this information helps.

Regards,

David

0 Kudos
Reply