Is MPX2102 waterproof

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is MPX2102 waterproof

Jump to solution
2,491 Views
Troyson
Contributor I

Hi NXP Team,

      We are choosing a pressure sensor which is used to test the pressure of gas and MPX2102 is suitable for us. The gas maybe contain vapor for it is exhaled through the mouth. So I want to know if 

MPX2102 can support waterproofness. Otherwise . are there other nxp waterproof pressure sensors for recommending.Thank you!

0 Kudos
1 Solution
2,488 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Troyson,

 

The MPX2102 is available only with a default fluorosilicone gel that is not supposed to survive exposure to water vapor molecules. 

I would recommend considering another type with an improved media resistant gel (MPXAZ, MPXHZ, MPVZ series). 

For more information please refer to the AN3728.

 

Best regards,

Tomas

View solution in original post

0 Kudos
3 Replies
2,489 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Troyson,

 

The MPX2102 is available only with a default fluorosilicone gel that is not supposed to survive exposure to water vapor molecules. 

I would recommend considering another type with an improved media resistant gel (MPXAZ, MPXHZ, MPVZ series). 

For more information please refer to the AN3728.

 

Best regards,

Tomas

0 Kudos
2,484 Views
Troyson
Contributor I

Hi Tomas ,

       Thank you for your great supports. Can I think that MPXAZ, MPXHZ, MPVZ series sensor can supports the gas which is in high humidity ? Thank you!

0 Kudos
2,473 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Troyson,

 

Yes, those series operate more reliably in high humidity conditions.

 

Best regards,

Tomas

0 Kudos