Is MPL3115A2 is bio-compatible ? https://www.nxp.com/docs/en/fact-sheet/MEDPRESSENSFS.pdf - recommend for wound management but could not find bio-compatible info in datasheet. Help to understand. Thanks in advace.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is MPL3115A2 is bio-compatible ? https://www.nxp.com/docs/en/fact-sheet/MEDPRESSENSFS.pdf - recommend for wound management but could not find bio-compatible info in datasheet. Help to understand. Thanks in advace.

1,860 次查看
chandann
Contributor I

Looking for a biocompatible pressure sensor for pressure measurement in the range of 0 to 300 mmHg in a smaller package (other than MPX2300DT1).

0 项奖励
回复
2 回复数

927 次查看
biomedical
Contributor I

When is FXPQ3115BV going to become active for production state. It still shows in development. 

0 项奖励
回复

1,117 次查看
reyes
NXP TechSupport
NXP TechSupport

Dear Chandan N,

 

As previously answered in your case. MPL3115A2 is not part of our medical certificated pressure sensors, so, there is no Bio-Compatibility information for this device. For your application, I rather recommend you to use the FXPQ3115BV which is designed for medical applications. The MEMS and ASIC die are coated with a biomedically-approved gel. The gel is a nontoxic, nonallergenic elastomer which meets all United States Pharmacopeia (USP) biological testing class VI requirements.

Datasheet for the FXPQ3115BV: https://www.nxp.com/docs/en/data-sheet/FXPQ3115BVSDS.pdf

The material composition declaration for this device can be found in the following link: https://www.nxp.com/mcds/FXPQ3115BV.pdf

 

I’m afraid that the full product specification for the FXPQ3115 is marked as a confidential document, so it cannot be shared without a signed NDA with your NXP sales representative or Distributor.

 

This device is still under pre-production, I recommend you to contact your local distributor for more details regarding availability for this device.

 

You can find details of the NXP Authorized distributors in the following link: https://www.nxp.com/support/sample-buy/distributor-network:DISTRIBUTORS

 

Have a great day,

Jose

NXP Semiconductor


-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复