Initialization of sensor fusion sometimes hangs in MPL3115_Init ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Initialization of sensor fusion sometimes hangs in MPL3115_Init ?

跳至解决方案
2,931 次查看
remibeges
NXP Employee
NXP Employee

I have noticed from time to time my application hangs on startup using the sensor fusion. I first suspected my code but then I noticed something.

After several seconds of execution, pausing the execution with the debugger reveals that the program is looping forever in MPL3115_Init, waiting for I2C callback to send the 'sent' flag

 

67480_67480.pngUntitled.png

 

Debugger shows that MPL3115_I2C_Error is 0

 

I am using KL46Z

My code is not interacting with any of the sensors or I2C so far.

Any idea of what is going on ?

标签 (1)
0 项奖励
回复
1 解答
2,554 次查看
michaelestanley
NXP Employee
NXP Employee

J7 on the shield is the jumper I was referring to.  It's right next to the Bluetooth module.

And yes, bad solder joints can also have the symptoms you describe.  And I guarantee the software will hang if you remove the shield.

在原帖中查看解决方案

0 项奖励
回复
8 回复数
2,554 次查看
michaelestanley
NXP Employee
NXP Employee

Which sensor board are you using?  The 9-axis board does not include an MPL3115A2.  If you have a 9-axis board, or don't need the MPL3115A2 for your app, comment out the line that says "#define USE_MPL3115A2" in build.h.

0 项奖励
回复
2,554 次查看
remibeges
NXP Employee
NXP Employee

Hi Michael, I am using this board, it does include the MPL_3115A2 :

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-FXS-MULT2-B

So far my application exchanges data with the computer through bluetooth serial port, and weirdly, the issue seems to happen more often when I leave the bluetooth serial port connected (led stays blue) and restart the debugging. I am not sure it is entirely related though, I need to make some more testing.

Is it even possible leaving serial port open on bluetooth might freeze the KL46Z I2C bus ? I find it unlikely

Is the MPL3115 the first sensor initialized or the first using I2C ?

I will try to find a consistent way to reproduce the issue

0 项奖励
回复
2,554 次查看
michaelestanley
NXP Employee
NXP Employee

Remi,

It probably has nothing to do with the MPL3115A2.  On the KL46Z, the same UART is routed to the Bluetooth module and used for serial communications over the OpenSDA.  If both try to use it, you will have conflicts.  Try removing the power jumper on the Bluetooth module when you are debugging and see if that resolves your problem.

Mike

0 项奖励
回复
2,554 次查看
remibeges
NXP Employee
NXP Employee

I tried removing the power jumper but then I don't receive anything at all on the usb serial port. I checked the port carefully, I am well connected to hard-wire serial.

Looking at the schematics of the shield, I believe I need instead to rotate the square jumper on UART_TX/RX in the bluetooth interface. Is that correct, can you confirm it Michael ? Haven't had the chance to test it yet

Also, I noticed an easy way to reproduce the I2C error is to remove the shield. So I suppose if a solder is bad on the KL46Z pin headers then result might be the same. I identified one potentially bad solder on the board header pins, I'll try to fix it and let you know the result

Thank you for your support

0 项奖励
回复
2,555 次查看
michaelestanley
NXP Employee
NXP Employee

J7 on the shield is the jumper I was referring to.  It's right next to the Bluetooth module.

And yes, bad solder joints can also have the symptoms you describe.  And I guarantee the software will hang if you remove the shield.

0 项奖励
回复
2,553 次查看
remibeges
NXP Employee
NXP Employee

I re-done a couple of solders, the problem seems gone now. Good news :smileyhappy:

0 项奖励
回复
2,553 次查看
michaelestanley
NXP Employee
NXP Employee

Excellent!

0 项奖励
回复
2,553 次查看
remibeges
NXP Employee
NXP Employee

I also forgot to precise that leaving the bluetooth serial port connected (and thus the bluetooth module as well) between two code runs definitely messes with the startup of the freedom board, you were absolutely right.

Basically the board never runs tasks in user_tasks.c if bluetooth is connected during flashing. However, during execution, I saw no issues using both KDS debugger with bluetooth serial port connected. I can debug my code just fine, and receive data just fine.

Just thought of sharing that feedback, might be useful to some other

0 项奖励
回复