Information about Sensor MPXV 7002dp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Information about Sensor MPXV 7002dp

1,466 Views
Prudent_pickle
Contributor I

Hi, 

I am writing on behalf of a group of researchers  to ask for information, if anyone have it available, about the sensor MPXV 7002dp since some parameters that we required are not specified in the data sheet, any information you can provide us is well received, please find attached a table with the parameters we are asking for we filled some parameters with the information available in the datasheet, the missing parameters are highlighted. Thank you very much in advance.

 

Parameter

Value

Measurement unit

Range (Rg): It is the extreme value width of a physical variable of a sensor in real time.

-2 – 2

kPa

Span (Sp): It is the diversified behavior of the physical variable.

4

KPa

Accuracy (Ar): The difference between the acquired

physical value and the actual value.

± 2.5

%VFSS

Precision (Pr): Closeness in acquired data with actual data is depicted in terms of precision.

 

 

Sensitivity (St): The variability in output generation for a physical variable in a stochastic environment.

 

1.0

V/kPa

Linearity (Lr): It is the fluctuation of the acquired

physical value and optimal data curve.

 

 

Hysteresis (Hr): Variation in the physical variable when input is altered between extreme points.

 

 

Resolution (Rl): Minimal alteration in the stochastic

environment acquired by the sensor.

 

 

Reproducibility (Rd): The capability of the sensor to

generate a similar output for the same input.

 

 

Repeatability (Rb): The ability to generate redundant data when repeated input is provided consecutively.

 

 

Response Time (Rt): It is delay is the generation of the acquired data value

1.0

ms

Labels (1)
0 Kudos
Reply
1 Reply

1,422 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Jose,

As you may noticed on the datasheet, the information that you requested is already characterized and covered on the accuracy parameter.

diazmarin09_0-1644881493647.png

I am afraid that it is all the information available from your request.

I hope this information will be useful for you.

Regards,

David

0 Kudos
Reply