Implementing NXP Hardware in Device Tree

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Implementing NXP Hardware in Device Tree

ソリューションへジャンプ
3,252件の閲覧回数
DillonM
Contributor I

I currently attempting to implement the mma8452 driver for my mma8451Q accelerometer by adding it to the the Linux Device Tree. 

Currently I am taking the route of creating a device tree overlay file (dtbo) that contains the addition to the device tree describing the accelerometer. It loads properly at boot and correctly pulls in the designated mma8452 driver. The driver however returns the following error in my dmesg log on boot:

 

[ 23.2352] mma8452: probe of 0-001c failed with error -121

 

Does anyone know what this means or how to fix it? Perhaps an overlay is not the correct way to do this and instead I should create a dtsi file or modify the source dts file? I can access the accelerometer from the console using the i2c-tools package at the SA0 address 0x1C. 

The driver supplied by NXP can be found here mma8452.c Driver 

My dtbo file can be seen below:

 

/*
 * MIRA custom cape device tree overlay
 * Supports MMA8451Q Accelerometer  
 */
/dts-v1/;
/plugin/;

#include <dt-bindings/interrupt-controller/irq.h>

/ {
        /*
         * Helper to show loaded overlays under: /proc/device-tree/chosen/overlays/
         */
        fragment@0 {
                target-path="/";
                __overlay__ {

                        chosen {
                                overlays {
                                        MIRA_EXTENSIONS = __TIMESTAMP__;
                                };
                        };
                };
        };

        fragment@1 {
                target = <&i2c0>;

                __overlay__ {
                        status = "okay";
                        #address-cells = <1>;
                        #size-cells = <0>;
                        accel@1C {
                                compatible = "fsl,mma8451";
                                reg = <0x1C>;
                                interrupt-parent = <&gpio1>;
                                interrupts = <16 IRQ_TYPE_EDGE_RISING>;
                                interrupt-names = "INT1";
                        };
                };
        };
};

 

 The target = <&i2c0> was chosen simply because it was an i2c node in another dtsi file. No other reason. May be wrong.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
3,233件の閲覧回数
DillonM
Contributor I

The solution was to target the correct i2c bus the Accelerometer was connected to. This ended up being i2c2, not i2c0. This solved my issue. 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,233件の閲覧回数
DillonM
Contributor I

The solution was to target the correct i2c bus the Accelerometer was connected to. This ended up being i2c2, not i2c0. This solved my issue. 

0 件の賞賛
返信
2,828件の閲覧回数
rockerr
Contributor III

Did you use the Yocto Project for your distribution? If so, could you explain how exactly did you manage to add your device tree to the linux-imx kernel source?

0 件の賞賛
返信