ISF 2.1 Install errors in windows 7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISF 2.1 Install errors in windows 7

1,644 Views
dkh
NXP Employee
NXP Employee


Hello,

 

We are getting errors trying to install ISF 2.1 in windows 7. Can you please provide some guidence ?

 

 

 

I am seeing errors when I try to install

 

 


33731_33731.gifisf 2.1 install errors.gif

Labels (1)
0 Kudos
Reply
1 Reply

1,210 Views
davidmunsinger
NXP Employee
NXP Employee

Hi Dennis,

I've been looking into this, but I cannot find a root cause.  The "Error: (9) The specified zip file was not found." may be related to Windows system error code:

ERROR_INVALID_BLOCK
9 (0x9)

The storage control block address is invalid.

But I can't be sure of that either.

The installer includes a set of temporary ZIP files that contain the content.  When the installer is done with placing the content in the final directory on disk, it deletes the ZIP file.  I can't tell from the output as to whether it is having problems on the creation in the target directory or just on cleanup.  Can you send me a picture of the resulting directory in C:\Program Files\Freescale\ISF_Kinetis\ISF_R2p1 and below?

thanks,

Dave...

0 Kudos
Reply