[IMX8M Plus] How to slove error messages related to ISP ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[IMX8M Plus] How to slove error messages related to ISP ?

974 Views
kengjian
Contributor I

1 I am tryimg to port a new camera(OV4689) for IMX8M Plus

2 refer to AN13713.pdf,download isp-imx and isp-vvcam(SDK version:L5.15.71_2.2.0)

3 isp-vvcam:

3-1 git clone https://github.com/nxp-imx/isp-vvcam.git -b lf-5.15.71-2.2.0

3-2 refer to os08a20,add OV4689 driver to "isp-vvcam/isp-vvcam/vvcam/v4l2/sensor/ov4689"

3-3 add private ioctl for OV4689

3-3 export KERNEL_SOURCE_DIR=/home/keng/imx8mp/kernel/linux-imx/

3-4 ./build-all-vvcam.sh v4l2

3-5 scp modules/*.ko root@192.168.12.10:~

3-6 update .ko to /lib/modules/[kernel git commit id]/

3-7 reboot the system

4 isp-imx:

4-1 wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/isp-imx-4.2.2.19.0.bin

4-2 ./isp-imx-4.2.2.19.0.bin --auto-accept

4-3 refer to os08a20,add OV4689 code(drv and xml) to isp-imx/isp-imx-4.2.2.19.0/units/isi/drv/ov4689/

4-4 ./build-all-isp.sh Release Full

4-5 scp -r build_output_release_Full/ root@192.168.12.10:~

4-6 update build_output_release_Full/opt/bin to /opt/imx8-isp/bin/

4-7 reboot the system

4-8 check the isp service(ps -x | grep isp)

kengjian_0-1707029795925.png

4-9 run test app (/opt/imx8-isp/bin/video_test -w 2688 -h 1520 -f RAW8 -t 2 -m 0)

kengjian_1-1707029811149.png

 

4-10 The error message is as follows:

kengjian_2-1707029828660.png

 

 

May I ask which step is causing the problem?Unable to locate the code location of the error message

May I ask if you can provide some ideas?Thank you very much!!

 

 

0 Kudos
Reply
2 Replies

950 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You have to build the full-image in yocto, it coming with the ISP-imx.

regards

0 Kudos
Reply

938 Views
kengjian
Contributor I
Hello:
1. I know that isp-imx and isp-vvcam are build by yocto
2. The above process is not related to whether it is in yocto or not(the same transplantation method),
and AN13713.pdf explain how to add new camera
3. I'm just not sure where this error message comes from,maybe it's isp_media_server
4. Attempted to add pr_info to the kernel driver(ov4689.c in isp-vvcam),It looks like it's working properly
5. If the key code of the error message can be located, it should be able to solve this problem

Can you provide some ideas or methods? Looking forward to your reply!
0 Kudos
Reply