I2C port and need to talk to I2C sensors over rs-485. Chip is available to convert from I2C to rs-485 but I don't see a chip to deconvert from 485 to I2C. There is one that receives rs-232 and is a bus controller but can't find one with a 485 interface.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I2C port and need to talk to I2C sensors over rs-485. Chip is available to convert from I2C to rs-485 but I don't see a chip to deconvert from 485 to I2C. There is one that receives rs-232 and is a bus controller but can't find one with a 485 interface.

621 次查看
tomkearns
Contributor I

Have an I2C port and need to talk to I2C sensors over rs-485.  Chip is available to convert from I2C to rs-485 but I don't see a chip to deconvert from 485 to I2C.  There is one that receives rs-232 and is a bus controller (need that clock output) but can't find one with a 485 interface.  Is there one or another approach?

0 项奖励
回复
0 回复数