How to port Arduino's max30100 heart rate sensor module function?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to port Arduino's max30100 heart rate sensor module function?

2,265 Views
ROSELJR
Contributor I

I found the program of Arduino's MAX30100 module from the Internet and wanted to use STM32 to do it all the time, but it got stuck in the millis function.

Please help me, thank you.

0 Kudos
Reply
1 Reply

2,260 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear RoselJr,

could you please confirm what part numbers you are referring to? The MAX30100 is a Maxim Integrated Pulse Oximeter and Heart-Rate Sensor IC, but in the link you provided, there is our PCF8575 I/O Expander on an Arduino board. The MAX30100 is not mentioned there. 

BTW, unfortunately we do not know MAX30100 and STM32, and we do not support them. I can try to help you with the PCF8575. Please specify your question.

With Best Regards,

Jozef

0 Kudos
Reply